Choose a country or area to see content specific to your location
白皮书
Summary
Changing from 34970A to 34972A can be as simple as an address change when using VISA I/O library software. For example, VISA address (A) shown below points to a 34970A on a GPIB address. VISA address (B) points to a 34972A on LAN. Changing from the 34970A to the 34972A can be as simple as changing just one address line.
Also, if needed the 34972A can respond to a *IDN? query with a product number of 34970A. So, there is no problem in the event you hard coded the software to only accept only a 34970A response. This white paper describes how simple it is to migrate to the new 34972A.