Choose a country or area to see content specific to your location
应用文章
Introduction
This application note presents the results of nanomechanical tests in which a Keysight Nano Indenter G200 was used to measure the force and displacement while crushing single ceramic particles. Two types of particles were provided for testing.
Experimental Setup and Procedure
Pieces of glass microscope slides (approximately 1cm x 2cm) were mounted to an aluminum stub using Crystalbond, which is a low-melting-temperature wax. After the stub and glass cooled to room temperature, a toothpick was used to deposit particles on the slide. The toothpick was inserted into the container and then tapped lightly at several points around the glass to deposit particles.