Choose a country or area to see content specific to your location
应用文章
Piezoelectricity
The Greek word “piezo” means pressure. In 1880, the brothers Jacques and Pierre Curie (18 and 21 years old!) reported on a discovery that the following year W. G. Hankel called piezoelectricity, a descriptive name for the phenomenon, in which mechanical stress applied to a sample of some materials apparently creates electric charge on certain surfaces of the sample.1,2 The total charge of the sample remains unchanged by the piezoelectric effect, but as a result of the mechanical stress, surface charge density is created.3 If a conductive material covers the charged area, and a conductive path exists from there to an electrometer, a charge of equal in magnitude registers in the electrometer, but that charge belongs to the conductors, not the sample.