Choose a country or area to see content specific to your location
白皮书
Need for network digital twins
Digital twin technology offers significant value to an organization as it allows continuous access to the digital replica of a physical object or process throughout its lifecycle. The digital replica can be used for analysis, which can provide insights and actionable information to improve the process or product in terms of optimized performance, cost effectiveness, readiness, or maintenance. A particularly strong use case for the digital twin approach is its use in communications and networking, commonly referred to as a network digital twin. A network digital twin is a computer simulation model of the communication network integrated with its operating environment and the application traffic carried by it. To satisfy its intended purpose, the network digital twin must have sufficient fidelity to accurately reflect the network dynamics due to the interplay between the communication protocols, topology, traffic, and physical environment. A network digital twin can be enhanced by incorporating cyber vulnerabilities and defenses. The cyber-enhanced network digital twin can be used to assess the cyber resilience of the target system by subjecting the digital twin to live or simulated cyber attacks and analyzing its behavior and resilience under a diverse collection of attack scenarios.