Accurate scattering measurements provide insight into how real materials interact with light. By incorporating measured optical properties into simulations, engineers can:
Our in-house laboratory is light- and temperature-controlled to provide an optimal measurement environment. Get the following SmartStart Measurement Services from our optical experts:
Accurate optical simulations depend on accurate input data. Keysight optical scattering measurements help engineers characterize real materials and surfaces, enabling more realistic models for imaging, illumination, and stray-light analysis. The result is greater confidence in design decisions before hardware is built.
Modern automotive and satellite systems rely on precise optical performance, where stray light and reflection can compromise reliability. Bidirectional Scattering Distribution Function (BSDF) measurements provide the key to understanding and controlling how surfaces interact with light.
We perform SmartStart Measurement Services from our in-house laboratory. The laboratory has strict temperature and humidity regulation, helping ensure the accuracy of your custom measurements. Specific services include 2D and 3D BSDF, high-resolution BSDF, TIR measurements, TIS measurements, and more.
The SmartStart Libraries store hundreds of optical measurements. We continuously augment our SmartStart Libraries to expand your access to precision light scattering data for faster, physics-based system modeling. LightTools and LucidShape offer SmartStart Libraries containing materials and media commonly used in the design of optical systems. This helps you save time and reduce development costs.
Scattering measurements help engineers understand how real surfaces and materials interact with light, improving simulation accuracy and optical system performance.
Measurements can be performed on optical coatings, lenses, diffusers, films, plastics, painted surfaces, mechanical components, and other materials used in optical systems.
BSDF is a general term describing how light is scattered. BRDF characterizes reflected light, while BTDF characterizes transmitted light.
Yes. Measured scattering data can be incorporated into optical simulation workflows to improve model accuracy and increase confidence in design decisions.
They help identify sources of unwanted reflections, flare, glare, haze, and stray light that can degrade optical performance.
Yes. Accurate scattering data is often used to create more realistic stray-light and ghost-image simulations.
Keysight supports measurements across ultraviolet, visible, and infrared wavelength ranges.
They can provide value during material evaluation, prototype development, design validation, manufacturing qualification, and failure analysis.
Yes. Our team can help transform measurement data into models suitable for engineering analysis and optical simulations.
Applications include automotive, aerospace and defense, AR/VR, consumer electronics, medical devices, industrial optics, and photonics.
Light scattering is the way light behaves when it interacts with a medium that contains particles or a boundary between different mediums that contains defects or structures. It is different than the effects of refraction, where light undergoes a change in index of refraction as it passes from one medium to another, or reflection, where light reflects back into the same medium, both of which are governed by Snell’s law.
BSDF stands for Bidirectional Scattering Distribution Function, which is a mathematical function that characterizes how light is scattered from a surface.
In an optical design, total internal reflection (TIR) bidirectional scattering distribution function (BSDF), also called internal BSDF, corresponds to a bidirectional scattering distribution function measured at an interface that separates two different mediums. The aim is to measure surface scattering from the inside of a material. It’s especially relevant for materials with a rough surface where surface scattering and total internal reflection phenomena occur together on two separate mediums. See the image for an example of a light guide with VDI texture modeled in LightTools.
Total integrated scattering (TIS) describes how much light is deviated (or scattered) from the incident light direction by diffuse reflection and transmission from a surface or optical element. It is equal to the ratio of diffuse reflected and transmitted optical power to the incident optical power when light is incident upon a surface.
Haze is one of multiple quantities that can characterize a diffusive material. The other quantities are reflectance, transmittance, absorption, total integrated scattering (TIS) measurements, and bidirectional scattering distribution function (BSDF).
Volume scattering is a phenomenon that occurs in an optical medium (e.g., glass or plastic), where the presence of small particles within the volume of the material causes light to scatter. Particulate flaws in the medium may occur due to small bubbles, inclusions, or contamination.
Reflectance describes how much light is reflected from a surface or optical element. It is equal to the ratio of reflected power and incident power when light is shot onto a surface.
Transmittance describes how much light is transmitted from a surface or optical element. It is equal to the ratio of transmitted power and incident power when light is shot onto a surface.
Spectral measurement is the process of analyzing the distribution of light intensity as a function of the incident wavelength. In the context of optical scattering, it involves measuring how light of different wavelengths is scattered by a material or surface.
何をお探しですか?