ISO Registrations: ISO 42001 English (full certificate)
Security Exhibits
DEKRA hereby confirms as a result of the certification decision on the issued date of this certificate according to ISO/IEC 17021-1 that the Artificial Intelligence Management System (AIMS) and implementation of: Keysight Technologies. Operates in compliance with the requirements of ISO/IEC 42001:2023 and is running the AIMS fulfilling the requirements of and is monitored by the DEKRA during the term of this certificate. This AIMS certificate doesn’t authorize the labelling of products, processes, and services.