Case Studies
Tower Semiconductor customers design photonic integrated circuits (PICs) on Tower’s PH18 silicon photonics process. With Keysight Advanced Design System (ADS) Photonic Designer certified for PH18 process design kits (PDKs), they work in one environment. They can simulate the full signal path across electronic and optical domains before tapeout, for applications such as co-packaged optics (CPO) and near-packaged optics (NPO).
The convergence of electronics and photonics for applications such as CPO and NPO is driving a new generation of high-bandwidth, low-power communication systems. By bringing Tower’s PH18 silicon photonics foundry technology into the Keysight ADS environment, we are enabling designers to model, simulate, and optimize complete electro-optical systems with greater accuracy and efficiency. This collaboration builds on our decade’s long partnership with Keysight and helps our customers shorten development cycles, reduce design iterations, and accelerate the deployment of advanced silicon photonics solutions.
As optical link rates climb to 1600G and beyond, performance depends on how electrical and optical behavior interact. Verification has to cover both the PIC and the system in which it will operate. Until now, that meant design teams worked in separate tools, transferring data and translating models between them.
Keysight certified ADS Photonic Designer to support Tower PH18 silicon photonics PDKs. Teams already using ADS for high-speed digital and radio frequency (RF) projects can now design PICs on Tower processes, or co-design them with electronic circuits, in the same tool. Designers place PH18 photonic circuits in the same schematic as their high-performance electronic circuits.
Tower customers can now simulate the complete signal path across electronic and optical domains before tapeout. Instead of moving data and translating models between separate tools, they model, simulate, and lay out electro-optical designs in one environment. “Photonic integrated circuits are becoming central to high-speed data communications, and the cost of getting the design wrong keeps rising.
Tower Semiconductor customers building PICs for high-bandwidth, low-power communication systems needed to verify electrical and optical behavior together, without moving data and models between separate tools. With ADS Photonic Designer certified for Tower PH18 PDKs, designers work from schematic through simulation and layout in one environment and can co-design photonic and electronic circuits. The collaboration extends a partnership of more than a decade between Tower and Keysight.
尋找感興趣的產品?