Power Amplifier Load Pull Design Techniques Leveraging Measurements and AI/ML

影片

Power amplifier designers often need to work directly with measured load pull data.  

 

Learn how Keysight’s ADS platform can: 

  • Import measured load-pull data
  • Clean up the data
  • Visualize contours
  • Use the data to design and optimize impedance-matching networks, including fitting ANN models that can be used in nonlinear simulations.  

 

This presentation will show several practical examples of using Load Pull data to optimize the key metrics of Power-added Efficiency (PAE), Error Vector Magnitude (EVM), and Adjacent Channel Leakage Ratio (ACLR) in a Power Amplifier design.