Harnessing Retail Media Networks and First-Party Customer Data

白皮書

Retail media networks (RMNs) are transforming the retail landscape, enabling retailers to monetize their first-party data in unprecedented ways. In the United States alone, RMN ad spend is projected to reach $109.4 billion by 2027, with profit margins between 50% and 90%, offering a compelling opportunity for an industry long reliant on slim operating margins. However, the difference between achieving 50% versus 90% profit depends on strategic execution.

This white paper explores the history, opportunities, and challenges of RMNs, offering actionable strategies to maximize their potential. It delves into the factors that enable retailers to position their RMNs as highly efficient, profitable revenue streams, while addressing barriers to success in three key areas: strategy, systems, and people.

 

The Evolving Media Landscape

The retail and advertising landscapes have changed dramatically. For brands, reaching fragmented audiences has become costlier and more complex, exacerbated by the deprecation of third-party cookies and the rise of privacy regulations. Retailers, meanwhile, face persistent inflation, post-COVID behavioral shifts, and global economic challenges. Amid these pressures, loyalty programs containing rich first-party data have emerged as a critical asset, offering opportunities for personalized targeting and new revenue streams.

 

The Rise of Retail Media Networks

RMNs appeal to brands by providing precise, measurable advertising opportunities. For retailers, RMNs generate new revenue with exceptionally high profit margins, poised to overtake traditional advertising channels such as linear TV. However, building scalable, efficient RMNs requires moving beyond reactive, tactical implementations toward comprehensive strategic planning.

 

Barriers to RMN Success

 

Strategic Barriers

Retailers must treat RMNs as distinct business ventures requiring robust go-to-market strategies. Defining unique selling propositions, business models, and key performance indicators is critical, as is ensuring the quality, organization, and security of first-party data. Many retailers face challenges with siloed or poorly managed data, which undermines their competitive edge.

 

Systems Barriers

The integration of RMNs into existing IT infrastructure presents practical challenges, such as managing hundreds of systems and ensuring scalability. Advanced platforms must handle complex deal configurations and deliver detailed metrics to brands to validate ROI. Automation plays a vital role in overcoming these barriers, reducing manual work and accelerating testing processes.

 

People Barriers

Successful RMNs require cultural and structural shifts within organizations. Teams must adopt new roles, develop cross-functional collaboration, and upskill to meet RMN demands. Retailers must also address customer concerns about data privacy, ensuring robust governance and creating a clear value exchange to maintain trust and loyalty.

 

The Path Forward

Retailers that invest in scalable, strategic RMN infrastructures can achieve profit margins closer to 90% than 50%. With limited market potential and increasing consolidation of brand spend into fewer RMNs, competition will intensify. Retailers must differentiate their offerings through superior data quality, seamless integration, and best-in-class analytics.

By adopting a proactive, strategic approach today, retailers can secure a leadership position in this transformative space, ensuring long-term profitability and competitive advantage in the evolving retail and media landscape.