尋找感興趣的產品?
5G and Satellite Communications Seminar
Join Keysight for a comprehensive overview of the latest developments in wireless communications testing. Local Keysight experts will be in attendance to demonstrate the latest in Keysight's 5G and satellite testing solutions.
AGENDA
9:00 a.m. / Registration
9:30 a.m. – 10:20 a.m.
Rapid RF Measurements
Learn about RF measurements and testing for the latest wireless technologies, including 5G NR and Wifi-6/7, and discuss the ecosystem driving these technologies forward, the challenges they bring to RF testing, and the Keysight solutions that reduce the time and effort needed to develop comprehensive test plans.
10:20 a.m. – 10:30 a.m. / Break
10:30 a.m. – 11:20 a.m.
Dual Sim Testing
Learn about the increasing use of Dual SIM Dual Access solutions in 5G devices that can leverage two independent network connections to provide more seamless connectivity and high reliability for its users.
11:30 a.m. – 12:30 p.m.
Field to Lab
Learn about how Virtual Drive Testing can be used to move device testing from a lab environment to a real-world environment, allowing its performance and functionality to be verified before it ever reaches the consumer.
12:30 p.m. / Lunch
12:30 p.m. – 1:30 p.m.
5G Non-Terrestrial Networking
Learn about the new developments that are enabling cellular wireless technologies to expand coverage through the use of non-terrestrial, satellite based networks, and discuss the challenges they bring to the device development and testing.
Dates and Locations
Tuesday May 23, 2023
Archer Hotel
3121 Palm Way
Austin, TX 78758
Tuesday June 20, 2023
Embassy Suites Chicago / Schaumburg
1939 N. Meacham Road
Schaumburg, IL 60173
Have questions or need help?