Choose a country or area to see content specific to your location
アプリケーションノート
Atomic force microscopy (AFM), a key member of the scanning probe microscopy (SPM) family, has developed into an invaluable tool of significant importance in many different areas of research and industry. Since its first development in 1986 [1] AFM has undergone much advancement, not only to extend measurement capabilities and to increase acquisition speed, but also to make the instrument more robust and user-friendly. Most commercial AFM systems today still use optical deflection detection to image samples of interest with nanometer resolution. Whereupon easy to handle and user-friendly self-sensing cantilevers are still mainly limited to home-built systems and special applications. Therefore SCL-Sensor.Tech. Fabrication in close collaboration with Keysight developed a hardware kit, making the benefits of user-friendly and easy to handle self-sensing cantilever technology available for Keysight AFM customers. In this application note a brief technical background of self-sensing cantilevers and the developed Converter Unit (CU) is introduced. Some representative images acquired with different modes of readout and excitation are also provided. In addition, the capability of using self-sensing cantilevers to image biological samples in different media including dry state, deionized water, physiological relevant buffer solutions, as well as non-transparent liquid are also demonstrated.
コンテンツのロックを解除する
無料でお申し込み頂けます
*Indicates required field
ありがとうございました。
フォームが送信されました。
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.