IcedID ISO File transfer

Strike ID:
C22-Mehf1
False Positive:
f
Variants:
1
Year:
2022

Description

This strike simulates the network transfer of the IcedID iso. When executed this malware mounts to the DVD drive on the machine containing a shortcut lnk and the IcedID malicious dll. Once the shortcut is executed the dll is loaded.

References