E16-66d01
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2016
Description
This strike exploits a remote code execution vulnerability in Adobe Flash Player.
The vulnerability is due to an out-of-bound memory access in the DeleteRangeTimelineOperation class.
An attacker can entice a target to open a specially crafted flash file to trigger the vulnerability. Successful exploitation may result in execution of arbitrary code or abnormal termination of the flash process.