Maximizing Success in Multi-Vendor Private 5G Networks

白書

The Private 5G market is still at the early stage of enterprise deployments, let alone real industry 4.0 production deployments. Today, Private 5G networks are typically single-vendor solutions deployed in ports, transportation, or mining with limited 5G requirements, mainly addressing WiFi shortfalls like handovers and range. As Private 5G deployments advance to delivering capabilities including immersive experiences, time-sensitive networking and process automation in smart factories, automated guided vehicles (AGV), and robotics, reliable networks with stringent SLAs will be required. Performance monitoring and assurance will need to not only quickly detect problems but predict or anticipate potential issues. 75% of manufacturers say 5G is a key enabler of their digital transformation strategy, according to Capgemini’s global enterprise survey.1 A new approach to assurance is required to enable 5G’s most disruptive features – high capacity, wireless flexibility, and low-latency performance – to support the industrial digital future.