Negative Testing using LoadCore

アプリケーションノート

Problem: How to simulate a realistic environment which contains a mix of traffic types, including illegitimate or malformed packets? 

 

5G is positioned to change the world in multiple ways, it is expected to form the foundation of tomorrow's digital economy. To achieve these ambitious objectives, an important role is played by the network resiliency, an aspect equally important for both public and private networks. In real life, a 5G Network Function can receive traffic from multiple sources, either as a standard compliant or something that is wrongly sent, malformed or intentionally looking for vulnerabilities. Simulating this mix of control plane traffic is challenging as the test tool should offer full flexibility for manipulating an entire message or only a specific Information Element inside the packet at a certain moment within any control plane procedure.