Assessing Network Risk

白書

The change in today’s corporate digital landscape is immense and fast paced. It is a huge challenge to keep up and stay current. In the same vein, networks are increasing in complexity in order to meet market and organizational changes. This adds to your challenges, as elements that affect secure networks evolve so rapidly that it can be difficult to understand when you have outgrown your network infrastructure, potentially leaving your company at risk.

Most businesses, like yours, may not have sufficient time or resources to assess network risks or create and implement an organized, long-term network visibility plan. As a result, many organizations have taken a reactive approach to network construction and maintenance, causing their networks to become large patchworks of applications and hardware that have a much higher chance of failing when they are needed most.

As the industry leader in network security testing on a large scale, Ixia researchers have to stay on top of the latest threats and trends. This ensures that we can reliably help customers configure their network visibility while in operation and ensure long-term cost savings.