Choose a country or area to see content specific to your location
白書
If you will be upgrading or migrating to a next generation firewall, take the opportunity to also review your overall security architecture. You spend significant time and money to implement, maintain, and upgrade your security infrastructure. Make sure your security tool architecture is designed to maximize value and efficiency. Limit the risk of downtime to your network. Keep your applications strong. All these benefits start with the simple addition of a bypass switch. For more advanced architectures, add a network packet broker.
This paper examines how you can achieve these goals and implement a resilient security fabric— one that delivers a self-healing, highly-available security architecture to complement your nextgeneration firewall (NGFW).
Reduce the Risk of Downtime
Take a close look at your overall architecture and identify all of the potential points for failure or performance issues. With serial inline deployment, traffic is passed from one security appliance to the other, meaning a failure in any one of the devices can stop traffic flow and cause a network outage. For most organizations, the cost of downtime is substantial and can be used to calculate the return on investment of any project proposed to reduce it.
コンテンツのロックを解除する
無料でお申し込み頂けます
*Indicates required field
ありがとうございました。
フォームが送信されました。
お客様のアクセスは、ブラウザーのCookieの有効期限が切れるか、ブラウザーのキャッシュがクリアされるとリセットされます。コンテンツに再びアクセスするには、もう一度サインインししてください。
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.