The Path to CMMC Certification

解決方案簡介

Cybersecurity Maturity Model Certification (CMMC) is not a one-time project. It’s a multi-stage program that requires planning, resources, and a shift from reactive security to continuous, evidence-based assurance. This solution brief, drawn from Keysight’s commissioned primary research, presents a practical six-phase roadmap designed to help Defense Industrial Base (DIB) organizations move from uncertainty to audit-ready compliance.

 

The roadmap begins with scoping and self-assessment, focusing on identifying where Controlled Unclassified Information (CUI) resides and defining the assessment boundary. It then moves into a formal gap assessment, where organizations can use data-driven methods and automation to identify deficiencies and prioritize remediation. The brief covers the realities of remediation and documentation, often the most labor-intensive stage, followed by validation and continuous monitoring to ensure controls are not only implemented but consistently effective.

 

A key research insight highlighted in this brief is the industry’s reliance on periodic, manual assessments: only a small minority of organizations report using automated security validation to continuously test control effectiveness. This gap increases risk as requirements expand and audits become more consequential. The brief also addresses the formal third-party assessment stage, emphasizing why readiness and evidence matter when audit capacity is constrained and re-assessments can cause costly delays. Finally, it reinforces that CMMC must be sustained through ongoing monitoring, training, and continuous improvement to remain compliant over the certification cycle.

 

Throughout the roadmap, the brief references how cybersecurity, network visibility, and test solutions can support measurable progress and audit-ready proof. For deeper findings, timelines, and practical guidance, visit the full commissioned research white paper, The Power of Proof: Turning CMMC Compliance into Competitive Credibility.