Choose a country or area to see content specific to your location
白書
Virtual and augmented reality (VR/AR), Internet of Things (IoT), autonomous cars, and high-definition (HD) video streaming escalate the need for more and faster data, both in the core network and the data center. Consumers no longer tolerate even the smallest delay to data access. In some applications, such as autonomous driving and medical IoT devices, delayed communication can lead to life and death situations.
Data center networks need to move from 100 gigabit Ethernet (GE) to 400GE speeds to support the requirements of emerging technologies. Faster networking speeds require faster memory and faster serial bus communications. In addition to moving to 400GE speeds, data center operators need to move to the next generation of high-speed computing interfaces, such as Peripheral Component Interconnect Express (PCI Express® or PCIe®) and Double Data Rate (DDR) memory. Data center operators also need to consider new specialized interconnect technologies that offer alternatives to PCIe.
コンテンツのロックを解除する
無料でお申し込み頂けます
*Indicates required field
ありがとうございました。
フォームが送信されました。
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.