Choose a country or area to see content specific to your location
アプリケーションノート
LTE-Advanced is the evolved version of the Long Term Evolution (LTE) standard developed by 3GPP to meet or exceed the requirements of the International Telecommunication Union (ITU) for a true fourth generation (4G) radio communication standard known as IMT-Advanced. LTE-Advanced is defined in 3GPP Release 10 and in subsequent 3GPP releases. The LTE-Advanced specifications are focused mainly on achieving higher capacity with increased peak data rates, higher spectral efficiency, ability to handle a greater number of simultaneously active subscribers, and improved performance at cell edges.
This application note gives an overview of the following topics:
The focus here is on the LTE-Advanced air interface, although the 3GPP specifications also cover the core network standards and services.
コンテンツのロックを解除する
無料でお申し込み頂けます
*Indicates required field
ありがとうございました。
フォームが送信されました。
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
営業担当者からご連絡させていただきます。
*Indicates required field
ありがとうございました。
A sales representative will contact you soon.