Google Chrome LinkToTextMenuObserver CompleteWithError Use After Free

Strike ID:
E22-1g5y1
CVSS:
8.8 CVSS:3.1/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2022

Description

This strike exploits a vulnerability in Google Chrome. Specifically, LinkToTextMenuObserver holds a pointer to a RenderFrameHost object, but does not properly observe when FrameHost destruction events occur. Because of this, if an attacker manages to craft javascript in such a way that will destroy the frame host at the right time, a use after free condition can occur in LinkToTextMenuObserver::CompleteWithError. When this happens a denial of service condition, or potentially remote code execution, may occur.

CVE

References

Google