Enterprise Application Testing with Cloud-Based Device Farms

解決方案簡介

In today’s world, customers interact with enterprises using mobile applications. Need to make a payment? Order food? Book a flight? There’s an app for that. Competition in the app store is fierce. Customers can switch to a competitor by simply removing one application and installing a new one

 

Enterprises improve user satisfaction, digital trust, and customer retention by making sure their applications are high-performing. Their customers use various devices that run on different operating systems, so testing is vital for application performance

 

Using Cloud-Based Mobile Device Farms with Eggplant Test Automation Solution

 

Testing apps on a wide range of devices is challenging. The device mix changes frequently and maintaining a centralized test lab can be costly. Not only do you have to procure the devices, but you also need to manage remote access and user permissions, keep the devices cool and the batteries charged, and much more

 

Integrating Keysight’s Eggplant test automation solution with software-as-a-service (SaaS) mobile device farms eliminates these problems. Mobile device farms in the cloud host thousands of devices, allowing enterprises to test their apps on users’ actual devices. Using mobile device farms in the cloud, teams can focus on testing apps rather than managing various devices

 

By connecting Eggplant software with a mobile device farm, you can design and run mobile app tests on emulators, private devices, and public devices hosted in the cloud.  Instead of relying on bolt-ons, Eggplant software has native support for devices hosted in the cloud, so test automation engineers can design and run tests on these devices as if they were connected locally

 

 

Emulator

Public device

 Private device

Cost

Low

Medium

 High

Flexibility

High

High

 Low

Real-world testing

No

Yes

Yes

Shared

No

Yes

No

 

Unlock the full potential of test automation

 

Integrating Eggplant software with your SaaS mobile devices unlocks the full potential of test automation to accelerate releases

 

Using Eggplant’s visual approach to testing, you can test critical human actions to ensure that any visual clues meant for end-user interactions are intuitive. By testing at the user interface layer, Eggplant can spot visual errors that cannot be identified in the code, such as blue text on a blue background or display issues associated with different screen sizes and orientations

 

Eggplant’s model-based approach lets you create a digital twin of your system, including mobile apps and other digital assets, such as websites. Your users are rarely predictable, so Eggplant can test every possible end-to-end user journey using artificial intelligence (AI) and machine learning (ML) algorithms. It even auto-generates test cases and prioritizes the areas of your app that need testing the most, so you don’t have to