Article Reprints
Error vector magnitude is a critical parameter for power amplifiers. Here’s an approach that combines a VNA and VSG with a modulation-distortion application to overcome measurement challenges.
In wireless communication systems, power amplifiers (PAs) make a significant contribution to the quality attained in the RF chain. These components play a critical role in determining the condition of the communication service in terms of signal quality and battery life. PAs are positioned in the last stage of the transmission chain and generate the RF power that’s then transmitted over the antennas. PA designers aim to maximize linearity while maintaining a high level of efficiency. This balance is challenging to achieve across extremely wide signal bandwidths in the millimeter-wave (mmWave) frequency spectrum. To measure the nonlinearity of a PA under a modulated stimulus condition, the industry uses error vector magnitude (EVM) as a figure of merit (FOM) for in-band characteristics and adjacent channel power ratio (ACPR) for out-of-band characteristics. This article introduces an innovative method called modulation distortion (MOD) for characterizing the nonlinearity of a PA under modulated stimulus conditions.
Challenges in Device Characterization Under Wideband Modulated Signals
The introduction of 5G new radio (NR) means that designers need to perform EVM measurements using extremely wide signal bandwidths in the mmWave spectrum. A vector signal generator (VSG) combined with a vector signal analyzer (VSA) are traditionally used to measure EVM. However, it’s challenging to measure EVM with these test instruments due to several reasons:
Errors contributed by the stimulus
In the VSA method, the error vector is the value obtained when comparing the ideal signal with the measured signal for each constellation. The integrity of the signal source has a direct impact on the measurement result. The distortion of the generated signal needs to be lower than the distortion generated by the device under test (DUT).
The VSA method is also sensitive to I/Q imbalance and phase noise not normally created by the DUT. In addition, the signal-to-noise ratio (SNR) increases as the bandwidth (BW) of the signal gets wider and generates noise. Random noise at low power levels can result in less accurate and reliable EVM measurements.
Errors contributed by the receiver
To minimize any errors in the EVM measurement result, the input signal needs to be digitized using a signal analyzer that does not produce any nonlinear distortion. Furthermore, the noise floor of the receiver must be lower than the target signal. This is especially challenging to accomplish across wider signal BWs since the SNR of the receiver is also lower.
To manage the input level of the receiver chain, the attenuation and gain settings of a receiver chain need to be carefully controlled, which requires deep knowledge of the analyzer. Iterating across different input levels and settings to optimize receiver optimization slows down the measurement process.
Signal fidelity
In the VSA method, there are multiple ways to calibrate the test system. The most advanced technique compensates for the I/Q waveform so that the input signal is a flat response at the reference plane. This method may include an error, especially when the test signal has a wide BW and the DUT has poor mismatch.
MOD on a PNA-X VNA
Modulation distortion offers a new approach to overcome the measurement challenges associated with the VSA method. By combining the following PNA-X, VSG, and MOD application, users can characterize the nonlinear distortion of a device under a modulated signal and establish FOMs, including EVM and ACPR (Fig. 1).
Since the entire measurement setup is integrated into the PNA-X firmware, the user can easily configure the stimulus and establish the measurements. Also, the measurement leverages state-of-the-art calibration techniques for optimum accuracy.
On top of that, the MOD application enables users to access additional measurements besides the typical PNA-X measurements, such as S-parameters, gain compression, intermodulation distortion (IMD), and noise figure. The MOD application on the PNA-X also supports nonlinear distortion measurements under a modulated stimulus condition without the need to change the connection.
PNA-X Unique Implementation
Figure 2 shows the block diagram of the measurement system consisting of a PNA-X and a VSG:
All of the required configurations to make a measurement can be completed with the MOD software application integrated into the firmware of the PNA-X. Similar to other application software that runs on a PNA-X, measurements start by creating a channel. The channel contains all of the stimulus-response information as well as the calibration information required for the measurement.
The calibration of the measurement system plays a critical role when making an accurate measurement. The MOD method offers two different types of calibrations to accurately perform EVM and ACPR measurements:
After the MOD application measures the vector-corrected input and output spectrum with a corrected receiver and the desired modulated waveform, the MOD application processes the data by comparing the input spectrum and output spectrum. The technique is called spectral correlation.
尋找感興趣的產品?