Develop C-V2X with Confidence as 5G Matures

解決方案簡介

Challenges to Successful Development of C-V2X

 

As 5G continues to evolve, the test requirements for C-V2X will be a moving target. The ability to thoroughly validate the performance of C-V2X designs depends on a test platform that can perform RF, protocol and application-layer testing while staying current with changing test scenarios.

 

Fewer accidents and greater road safety are central to the vision for autonomous vehicles (AVs). That vision depends on technology that enables greater situational awareness: observing what’s happening, predicting what’s likely to happen, and automatically taking protective action. Getting there requires dependable communication via wireless technology that provides superior range, predictable performance, low latency, and high-speed connectivity. Cellular vehicle-to-everything or C-V2X has emerged as the wireless link that can help enable higher levels of autonomous operation.

 

C-V2X continues to take shape, in part because it is dependent on the evolution and deployment of fifth-generation (5G) wireless technology. As part of the 3rd Generation Partnership Project (3GPP) Release 14, C-V2X is focused on vehicle-to-infrastructure (V2I) communication. The goals of Rel14 C-V2X are to improve road safety, increase traffic efficiency, and support a growing range of traveler services.

 

Learn more, by downloading this solution brief on "SA8700A C-V2X Test Solution: Develop C-V2X with Confidence as 5G Evolves".