資料表
Introduction
Power converters are a key component enabling the electrification of the transportation, renewable energy and industrial markets. To facilitate needed advances in power converter design, new wide-bandgap (WBG) semiconductor technologies, based on silicon carbide (SiC) and gallium nitride (GaN), are being commercialized. WBG semiconductors provide major leaps in speed (10x to 100x faster than older designs), higher voltage and thermal operation, which in turn improve efficiency, reduce size and cost.
However, the resulting high-performance power converters are proving difficult to design due to many new challenges when characterizing WBG semiconductors. These difficulties delay the innovation of semiconductor manufacturers and engineers designing new converters.
Homegrown test systems have been the primary source for characterizing WBG semiconductors. Building these systems has been necessary because, to date, commercially available test systems have not been readily available. Unfortunately, it is difficult to produce repeatable and reliable measurement results with one-off, “homegrown” testers. Unreliable results create additional obstacles for power-converter designers when correlating their measurements with the semiconductor’s data sheets.
To enable consistent, reliable characterization of WBG semiconductors, Keysight created the PD1500A dynamic power device analyzer platform. Initially employing the Double Pulse Test (DPT) technique, it has been developed in close collaboration with semiconductor manufacturers and designers from the energy and electric vehicle (EV) industries.
Reduce your time to market with the PD1500A
As an off-the-shelf measurement solution, the PD1500A delivers repeatable, reliable measurements of WBG semiconductors. The platform also ensures user safety and protection of the system’s measurement hardware.
The ability to ensure repeatable DPT results is built on Keysight’s expertise in measurement science. Examples include innovations in high-frequency testing (gigahertz range), low leakage (femto-ampere range), and pulsed power (1,500 A current, 10 μs resolution). As a result, Keysight is uniquely positioned to help you overcome the challenges of dynamic power-semiconductor characterization.
Included with the PD1500A are standard measurement techniques such as probe compensation, gain/offset adjustment, de-skewing, and common mode noise rejection. These techniques are utilized within an innovative measurement topology and layout. A semi-automated calibration routine (AutoCal) that corrects for system gain and offset errors was specifically developed for this system. The system also uses advanced techniques to compensate for inconsistencies when measuring current.
Overview: Established and emerging measurement methods
Fully characterizing a SiC- or GaN-based WBG device requires both static and dynamic measurements. Keysight’s B1505A and B1506A power device analyzers excel at static measurements. The PD1500A has the needed flexibility to address a variety of dynamic measurements and the evolution of JEDEC standards as they take shape.
Static measurements: The following parameters are typically used to understand the static characteristics of a power device:
Dynamic power converter design challenges
Semiconductor and power engineering teams are in a tenuous position. The market forces them to quickly develop and ship reliable products, while needing to overcome changing technology, unreliable measurements in a hazardous test environment. In the absence of commercial characterization solutions, most engineering teams have been forced to develop their own solutions. Some of their key challenges are listed below:
尋找感興趣的產品?