Brochures
Eliminate noise oversight using Accelerated Time Domain Scan. High reliability measurement software comparable for skilled EMC engineers.
With the evolvement of IoT, 5G, autonomous driving and other technologies, the radio environment around us is becoming increasingly complicated. This means that the electromagnetic noise across these technologies needs to be evaluated and reduced during the product development process, making EMC measurements more important. TOYO Corporation has developed the EPX / RE, a radiated emission measurement software product for electronic equipment, including multimedia equipment, home appliances, medical equipment, etc. The "EPX/RE" achieves accurate measurements without noise oversight by incorporating the latest measurement technology, Accelerated Time Domain Scan, installed in the N9048B PXE.
High reliability measurement without noise oversight.
When the new Accelerated Time Domain Scan function is enabled, the FFT bandwidth is 350 MHz. This is much wider than the FFT bandwidth of the TDS function in existing products. You can measure the 30-1000 MHz band using only 3 range divisions. Additionally, there are no measurement gaps within the FFT bandwidth, since all the frequencies are constantly monitored. By incorporating the Accelerated Time Domain Scan into the automatic measurement sequence, we achieve reliable measurements without overlooking noise.
QP pre-scan with 350MHz FFT bandwidth
Accelerated Time Domain Scan maintains its wide FFT bandwidth of 350 MHz even when making measurements using QP detector. This has now made it possible to perform pre-scan measurements in the 30-1000 MHz band using QP detector. By picking up the noise of the final measurement candidate based on the pre-scan measurement results, using QP detector, you can suppress the pickup of unnecessary candidates such as impulses and reduce test points. Depending on the noise, it may even be possible to adopt the pre-scan measurement results as the final measurement.
Features
尋找感興趣的產品?