Overcome Massive MIMO Challenges for 5G

應用說明

Introduction

Consumers, businesses and developers have lofty expectations for fifth-generation (5G) wireless technology. One frequently used word is “massive,” as in massive growth in demand for mobile data, massive growth in the number of connected devices, and a massive explosion in the diversity of mobile applications.

Delivering on these expectations depends on the evolution of existing technologies and revolution in new technologies. One revolutionary change is in the use of massive multiple-input/multiple-output (MIMO) antenna schemes. All of this has implications for the development and implementation of massive MIMO technology within the 5G ecosystem. It also has implications for the hardware and software tools needed to simulate, design, and test highly complex systems containing tens or hundreds of antennas and the associated communication pathways.