Testing and Validation for LPDDR4 and DDR4 Memory

應用說明

DDR4 and low-power DDR4 (known as LPDDR4) comprise the most recent generations of Double Data Rate (DDR) SDRAM memory. DDR4 and LPDDR4 enable significantly higher bandwidth for data transfer than DDR3 and offer evolutionary improvements in speed, density and power over previous generation memory.

Designers are embracing the latest DDR4 and LPDDR4 memory technologies to increase system data rates beyond 2400 Mb/s and push designs to record speeds and power savings.