Monitoring and Controlling Particle Beams in Real Time

應用說明

High-performance digitizers enhance beam quality in advanced applications

High-energy particle accelerators are helping researchers investigate the nature of matter and the origins of the universe. Typical experiments involve carefully controlled collisions between either intersecting particle beams or a particle beam and an atomic-scale target. Subsequent analysis of the results may reveal new insights about the building blocks of matter and the forces that hold them together, answer questions about particles and dark matter, and provide clues about the formation of the universe more than 13 billion years ago.

Creating particle collisions at nanometer scale and with picoseconds of duration requires extreme precision in spatial and temporal control. At facilities such as the European Organization for Nuclear Research, more commonly known as CERN, and the Australian Synchrotron, high-performance Keysight Technologies, Inc. Acqiris digitizers are helping researchers achieve the levels of precision and control they need to perform more and better experiments in less time. Key attributes of the Keysight digitizers include high measurement throughput, very short “dead time” between acquisitions, excellent measurement fidelity, compact size and cost-effectiveness.