Brochures
When noise is present in test or characterization systems, it often leads to the question of whether the DUT is producing a noisy output in response to a stable input signal or responding to noise at the input. You can spend a lot of time and energy troubleshooting the DUT, only to discover that the signal being input to the DUT is the source of the problem. It is possible to filter the noise at the DUT input, but it is often easier to reduce or eliminate the noise before it ever reaches the DUT. Understanding some common sources of noise will make it easier to minimize the noise in your test..
Snapshot: Reducing noise in battery-powered device tests
In the wireless communications market, battery operating times are improving and batteries are becoming smaller and more efficient. To support these trends, digital wireless products transmit in short bursts conserving power between transmissions. When using a power supply in place of the battery for testing, a high-volume manufacturer of wireless products found that the short transmission bursts caused pulses of current to be drawn from the power supply resulting in voltage transients at the wireless product’s input and triggering the low-battery shut-down of the product. To avoid these disruptions in the test, the manufacturer minimized the impedance and noise in the lead wires by using low contact resistance relays and larger-gauge shielded twisted conductors.
Choosing a quality power supply
Using a low-noise power supply is the first step to keeping noise out of your test. Linear power supplies have a reputation for lower output noise and lower common mode current noise. Some switching power supplies, such as Keysight Technologies, Inc.
N6700 modular power system or N6705A DC power analyzer, have been designed to minimize noise by employing extensive filtering techniques and reducing stray capacitive coupling. When you select a power supply that has been designed to reduce
noise, it allows you to use a switching supply in applications where you previously may have thought only a linear design would have worked. A well designed switching power supply will have the low noise performance you would expect from a linear supply.
Normal mode voltage noise and common mode current noise
An ideal power supply has a perfect DC output with no AC signals across the output terminals or from the terminals to earth ground. In reality, power supplies have noise across the output terminals (normal mode voltage noise) and a flow of current through any impedance connected from either terminal to earth ground (common mode current noise).\
Normal mode voltage noise is in the form of ripple related to the line frequency in a linear design or the switching frequency
in a switching design, plus some random noise. Normal mode voltage noise is typically very low in a quality power supply. You can maintain the low noise performance by minimizing noise pickup.
Do this by keeping the power supply circuitry away from devices that consume large amounts of power and other noise sources such as large motors or relays switching large currents.
Common mode noise is generated when common mode current flows from inside the power supply through the output terminals to earth ground, generating a voltage drop across any impedance in the path. When multiple instruments are used, multiple paths to ground result. To minimize the conducted noise caused by ground loops, separate the DC distribution path from the other conductive paths that carry ground currents. You can also float the power supply by not referencing the power supply outputs to earth ground and eliminating the ground loop.
Changes in the Load
The DUT’s current demand can change very rapidly causing the DC output voltage of the power supply to also change in response. To reduce any voltage spikes at the DUT, connect a low impedance bypass capacitor close to the DUT input.
The inductance of the lead wires can also cause a voltage spike to appear at the DUT in response to rapidly changing currents. You can reduce this spike by keeping the load wires as short as possible and by bundling thewires together as tightly as possible.
Summary
Using clean power signals in your system improves the reliability of your test by reducing the chances that your DUT will fail due to a noisy signal at the input. We have reviewed ways to minimize or eliminate common sources of noise and reasons why using the right power supply, such as Keysight’s N6700 family of modular systems and the N6705A DC power analyzer, is a great first step.
尋找感興趣的產品?