Virtual Distortion Engineering for Automotive BiW

解決方案簡介

Automotive manufacturing is undergoing a fundamental transformation driven by electrification, lightweighting strategies, and increasingly stringent safety requirements. These trends are reshaping Body-in-White (BiW) architectures, which now incorporate advanced high-strength steels, aluminium components, and complex multi-material joints. As a result, manufacturing engineers must manage tighter tolerances across larger and more intricate assemblies, where even minor geometric deviations can propagate through the assembly process and lead to significant structural distortions.

 

Similar challenges are also present in adjacent industries such as heavy machinery and industrial equipment, where large welded structures demand high precision and structural integrity. Across these sectors, the need for robust and scalable assembly validation methods is growing as product complexity increases.

 

Traditionally, distortion and assembly issues have been addressed during physical try-out phases, where prototype builds are used to evaluate fit, fixture strategies, and welding sequences. While effective, this approach is resource-intensive, time-consuming, and highly dependent on access to physical tooling and production environments. Late-stage issue detection often results in costly design changes, fixture rework, and production delays—challenges that are increasingly incompatible with today’s compressed vehicle development timelines.

 

To address these limitations, manufacturers are shifting toward simulation-driven methodologies that enable earlier and more predictive validation of assembly processes. Virtual distortion engineering allows engineers to digitally model how component variations, clamping forces, and welding sequences interact, providing insights into distortion behavior before physical prototypes are produced.

 

This solution brief details how Keysight Assembly, part of Keysight’s CAE Manufacturing Suite, offers a specialized environment for simulating automotive assembly processes. It supports workflow-driven modelling, automated stamping geometry prediction, and physics-based analysis to evaluate assembly behavior in a virtual setting. By enabling engineers to identify and mitigate potential distortion issues early in the design phase, the solution reduces reliance on iterative physical testing and improves overall process efficiency.

 

As digital manufacturing continues to evolve, simulation-driven assembly validation is becoming a critical enabler of faster, more reliable, and cost-effective production. By integrating virtual distortion engineering into development workflows, manufacturers can better manage complexity, enhance product quality, and support the transition toward more sustainable and agile manufacturing systems.