How to Set Up Keysight PN3 Signal Source Analyzer Remote Connection

應用說明

This application note describes the different ways to establish reliable remote connection to your Keysight PN3 Signal Source Analyzer. 

 

The PN3 Signal Source Analyzer supports two different modes of operation: 

  • User mode via GUI (graphical user interface) 
  • ATE mode (control over SCPI commands) 

 

In both cases, remote connection to the signal source analyzer is required. Three different physical interfaces are supported: 

  • Ethernet LAN 
  • USBTMC 
  • GPIB (optional)