Wire Bond Electrical Structural Test Methodologies

白皮書

Wire bonding, a foundational process in microelectronics, is essential to establishing a robust and low-resistance electrical connection between semiconductor chips and their respective packages or, in the case of multi-chip modules, between different chips. This intricate process ensures the device's functionality, reliability, and overall performance.

 

Wire bonding faces several challenges that become more critical as technology advances. Firstly, the miniaturization in the semiconductor industry has led to shrinking components, significantly increasing the complexity of wire bonding processes. Secondly, the trend towards high-density packaging, aimed at integrating more functions per unit area, presents difficulties in wire placement and avoiding wire-to-wire shorting. Additionally, material compatibility issues can arise, where different materials might react over time, leading to degradation and potentially compromising the integrity of connections. 

 

Automated Test Equipment (ATE) is an advanced apparatus designed for automated electrical testing of wire bonds in semiconductor devices. Also, it can handle analog, digital, and mixed signals for injecting and measuring stimuli in a Device Under Test (DUT). 

 

If continuity tests reveal a significant voltage drop, it can indicate an open circuit. Similarly, unusually high leakage currents observed during leakage tests may suggest the presence of a short circuit. Resistance or impedance values that fall outside the specified limits could bring issues such as wear, tear, or inconsistencies in manufacturing, leading to degraded performance.

 

ATE is not comprehensive, it only tests electrical characteristics and fails to detect mechanical and structural defects such as sagging or misalignment. Additionally, its sensitivity is limited; although ATE can catch overt failures, it might not identify subtle long-term reliability issues. The potential for false positives and negatives also poses a challenge, as it can lead to unnecessary rework or the inadvertent passage of defective units, depending on the set pass/fail thresholds. 

 

X-ray imaging, or Automated X-ray Inspection (AXI), is a non-destructive testing methodology that plays a critical role in evaluating the quality and integrity of wire bonds in semiconductor devices. Unlike other inspection techniques, X-ray imaging can penetrate through the substrate material and capture hidden defects.

 

Conventional Radiography utilizes X-ray film that is exposed to radiation transmitted through the sample. The film is then developed using photographic techniques to create a static image of the internal structures.

 

Real-Time Radiography captures the X-ray image in real time, and the output is directed to a video display. This allows for real-time adjustments, rotations, and translations of the sample to optimize the perspective and information captured.

 

In wire bond inspection, X-rays can inspect the internal clearance, positioning, and spacing of bond wires within semiconductor packages, detecting issues like crossover and excessive bond tail length. For solder joint inspection, the technique can effectively identify defects such as cracks, voiding, head-in-pillow defects, and missing solder. X-ray imaging is also adept at detecting sealing issues, including seal ring voiding, fillet defects, and incomplete melting in seals. 

 

It is important to note that while X-ray imaging is a powerful tool, it has limitations that can affect its effectiveness. One significant limitation is its capacity for material differentiation. X-ray imaging primarily captures variations in density, making it difficult to distinguish between materials with similar densities. Additionally, it has limited sensitivity to certain features, such as aluminum wire bonds, which may not be easily detectable, leading to potential gaps in the inspection process. 

 

Capacitive testing utilizes Keysight's Vectorless Test Enhanced Probe (VTEP) technology, which was initially developed for printed circuit board assembly (PCBA). The VTEP method employs capacitive measurement techniques to test the connectivity of an IC or a connector to a printed circuit board without requiring the IC to be powered up. The approach capitalizes on the capacitive coupling characteristics between metallic surfaces —such as the lead frame and wire bonds within an IC — by placing another metallic plate, known as the sensor plate, above the IC. By doing so, each pin of the IC becomes a basic capacitor that can be tested.

 

Capacitive testing stands out as a non-invasive and non-destructive method that does not require powering up the device, thereby reducing the risk of damage during testing. It provides higher sensitivity, particularly with advanced technologies like VTEP, enabling the detection of defects such as "near shorts" that might go unnoticed by traditional ATE and X-ray methods. Additionally, capacitive testing is fast and efficient, allowing for quick scanning of each IC pin, which is particularly beneficial for screening large volumes of devices. 

 

The Keysight s8050 Electrical Structural Test (EST) Solution utilizes Keysight’s advanced nanoVTEP technology, employing capacitive and inductive sensing techniques and statistical analysis through part average testing (PAT). By establishing a baseline from a set of known-good units, it detects and captures outliers in wire bonds as deviations from expected standards.

 

The key features of the s8050 can support up to 2560 pin resources and enable up to 20 parallel sites per system. It also provides advanced networking via SECSGEM and facilitate communication through GPIB. Additionally, s8050 includes a built-in tester interface board for the instrument core, and DIB interconnect. With all these features, s8050 manages to conduct comprehensive testing with methods such as (Open & Short Test, nVTEP) and enhance yield improvement capabilities with retest bin, Marginal Retry Test (MaRT), Dynamic Part Averaging Test (DPAT) and Real-time Part Averaging Test (RPAT).

 

In pursuit of optimized production efficiency, the Keysight s8050 Electrical Structural Test (EST) system stands out with its ability to accommodate up to 20 parallel test sites. The high-level parallelism empowers it to achieve a testing capacity of up to 58,000 IC Units Per Hour (UPH), significantly boosting throughput in electronic package testing.

 

Moreover, the s8050 EST system effectively addresses Electrical Overstress (EOS) challenges that could affect chip integrity. Doing so aids manufacturers in delivering high-quality components, reducing product returns, and ensuring the reliability and consistency of electronic products throughout their lifecycle.