解決方案簡介
Elevate your 5G device test solution
5G is an exciting technical advancement – but it can also be a daunting one for QA teams. In comparison to its predecessors, 5G allows exponentially more data over the air for faster speeds, reduced congestion, and lower latency. Considering these improvements, 5G has added layers of complexity for testing. Therefore, it is vital to thoroughly test the performance of 5G devices in a variety of scenarios and use cases to ensure they are robust and able to handle the demands of real-world use.
尋找感興趣的產品?