Bypass Link Conveyor Built-in i7090 and i3070 In-Circuit Inline Tester

應用說明

An automated production line uses an external link conveyor to transport objects such as the Printed Circuit Board (PCB) from one station to another. In some instances, the production line may require two similar systems or more at a station to maximize the production output rate. In such a case, you must have an external bypass link conveyor to transport the PCB from the busy system to another available system to perform the task simultaneously. However, the external bypass link can be complex to design and difficult to implement. It could also significantly take up the floor space.