Device Modeling Solution for Quantum Computing

應用說明

A Quantum computer, which uses quantum phenomena to perform computation, is believed to be able to solve much more complex problems compared to a classical computer.

 

Device modeling, on the other hand, is well known as one of the basic components of technology computer-aided design. With the fast development of integrated circuit technology, device modeling is mainly focused on CMOS models, and it is always intended to create accurate models to fully describe device electrical behavior based on semiconductor physics.

 

Instead of CMOS technology in classical computers, the heart of quantum computing is the qubit. However, device modeling will still be used in different components of the quantum computing system. In this paper, we’ll discuss device modeling applications, challenges, and solutions in the world of quantum computing.