技術綜覽
Threat Simulation System Development
The workflow to test and evaluate an electronic warfare system will move in different stages from system simulation, to system integration, to hardware in the loop, to an installed system prior to open air range testing.
This process is:
Conducting RF tests that most resemble real-life conditions, early on in development, is very important as moving into open air range testing increases the cost of error.
Keysight has decades of RF expertise in test and measurement to help mitigate most of these issues.
尋找感興趣的產品?