Scenario files are provided for use with the N7609B Signal Studio for GNSS. All visible satellites are included in the scenario files, but an advanced capability license for GPS, GLONASS, Galileo, or Beidou must be installed in the instrument in order to simulate satellites from that constellation. The files do not require licenses for the scenario generator options RFP, TFP, or VFP.