Automotive Lidar (Light Detection and Ranging) Target Simulator
Lidar technology has come a long way from
its use in meteorology and topography. It is fast becoming an automotive sensor
that is both a key addition to advanced driver assistance systems (ADAS) and an
enabler of autonomous vehicles. The tremendous investment in lidar technology
in the automotive market is an indicator that it is poised for increased
adoption, but there are cost, quality, and time-to-market challenges to
overcome. Validation and testing will play a key role in addressing the
challenges impacting the future of autonomous vehicles.
Keysight’s lidar target simulator is an
exciting step into the future of lidar sensor testing. The compact design frees
up valuable space and its features offer powerful insights into lidar performance.
The solution enables you to do the following:
Simulate and automatically sweep in distance and reflectivity
Implement both solid-state and mechanical rotating lidar sensors
Perform 3D / real-world object simulation
Improve quality and yield with insights from innovative visualization and analytical software