白書
From accelerating the discovery of life-saving medicines to boosting the security of financial services, quantum computing's potential business opportunities seem limited only by the imagination. However, the tangible barriers quickly become clear for organizations actively using this rapidly emerging technology.
In their 2022 technology, media, and telecom predictions, consulting firm Deloitte likened the current state of quantum computing to aircraft technology in the early 1900s. At that time, the Wright brothers had found it was possible to get a plane off the ground, but they could not yet travel meaningful distances.
"The problem with quantum computing's usefulness is not a lack of use cases, money, effort, or even progress," Deloitte's analysts wrote. "It's that current quantum computers are not yet powerful enough to tackle problems that can't be performed by traditional [super]computers."
何をお探しですか?