Article Reprints
Introduction
What is the ideal Double Pulse Test (DPT) system?
A question we often ask as a test & measurement equipment manufacturer is ‘What is the ideal power semiconductor dynamic test or double pulse test system?’. There are many responses depending on the challenges people encounter at their work. But one of the typical answers for this question is something like this. Insert DUT to the system, push a button and then the system safely performs measurement with excellent accuracy. It is simple to say. However, it is not so easy to make the ideal DPT system.
何をお探しですか?