Posters
Vector signal generators (VSGs) produce digital modulation signals in today’s communication test systems. The VSG is one of the core test instruments used to verify and characterize the performance of an RF device. Minimizing measurement uncertainty in test systems begins with an understanding of the VSG’s capabilities, features, and performance levels.
A VSG has three main sections — a baseband generator (BBG), I/Q modulator, and RF output. Here are 7 common errors using RF vector signal generators and how to minimize them.
何をお探しですか?