800G / 1.6T Data Center Transceiver Test

白書

The AI revolution is redefining the landscape of data center performance, demanding unprecedented levels of network speed and efficiency. This white paper examines how hyperscale data center architects and operators must scale their infrastructures from legacy 400G networks to 800G and 1.6 terabit (1.6T) Ethernet speeds required for the next generation of AI applications.

 

This guide dives into three key hurdles facing transceiver manufacturers:

  • Increasing interconnect bandwidth
  • Ensuring interoperability and reliability for complex AI traffic
  • Reducing test time, power, and cost

 

The first challenge highlighted in the paper is the dramatic increase in data traffic due to AI workloads. AI clusters, often composed of hundreds of graphic processing units (GPUs) working in tandem, drive significant east-west traffic within data centers. This surge necessitates a robust and agile network architecture where each interconnect—ranging in the thousands to millions per facility—must operate reliably at high speeds. With each connection representing a potential weak link, even a single underperforming transceiver can have a cascading effect on overall system performance. Increasing interconnect bandwidth is critical. The evolution from non-return-to-zero (NRZ) signaling to four-level pulse amplitude modulation (PAM4) was pivotal in boosting speeds from 100G to 400G. However, the leap to 1.6T speeds requires the development of 224 Gb/s lanes, which brings new signal integrity issues as the data rates surge.

 

The second hurdle is ensuring interoperability and reliability across a heterogeneous mix of network components. For hyperscale data centers, it is imperative that new transceiver technologies not only comply with industry standards but also interoperate seamlessly with legacy systems and components from various vendors. The paper discusses how compliance testing—covering both physical layer (Layer 1) characterization and protocol/network layer validation—is essential for identifying potential performance issues before deployment.

 

The third challenge is about reducing test time, power consumption, and overall costs in the production and deployment of next-generation optical transceivers. The inherent complexity of testing devices that operate at 1.6T speeds is amplified by the increased number of lanes and the tighter margins required by advanced modulation techniques such as PAM4. The paper emphasizes the importance of automated compliance testing. High throughput testing methods, combined with optimized hardware utilization and sophisticated optical test software, are crucial for reducing the time and power required for comprehensive device characterization.

 

Beyond the technical challenges, the white paper addresses the broader implications of these advancements for the future of data center design. As AI continues to drive exponential growth in data volume and processing demands, the ability to scale networks from 400G to 1.6T becomes not just a technical challenge but a strategic imperative. Hyperscale data center operators must adopt innovative solutions to build resilient, high-performance infrastructures capable of supporting AI-driven workloads.