S-parameter Series: Transforming Oscilloscope Acquisitions for De-Embedding, Embedding and Simulatin

アプリケーションノート

Introduction to Signal Acquisition and Theory

This paper is the first of 6 papers whose intent is to guide designers and validation engineers of highspeed digital systems through the details of channel element measurement and modeling for the purpose of manipulating oscilloscope acquisitions to reveal the signals that the engineer wants to see and measure. This extra processing is required because the actual signal cannot be probed (for various reasons) or because the probed location is different than is desired, or because the measurement elements themselves (i.e. probes) affect the measurement result and need to be removed from the reported measurement.