アプリケーションノート
Keysight B1500A Semiconductor Device Analyzer
Exotic carbon nanotube (CNT) structures have generated a great deal of interest in the scientific community. There are many potential applications for CNTs, but much of the current focus in nanotechnology research is centered on electrical component structures, such as the CNT field effect transistor (FET) and the CNT single electron transistor (SET).
The Keysight Technologies, Inc. 4155C and 4156C have been the de facto industry standard instruments for semiconductor device characterization for many years. In addition, they are very effective tools for nanotechnology device characterization. However, the new Keysight B1500A Semiconductor Device Analyzer is also an excellent instrument for analyzing the electrical properties of nanotechnology devices, and it has added benefits not found in the 4155C and 4156C.
何をお探しですか?