Posters
The "Function Generators In the Lab" poster demonstrates how Keysight’s EDU33210 Series SBE Waveform and Function Generators are made easier for customers to use in the lab. It includes quick setup tips that illustrate the process of operating the function generator.
Additionally, the poster highlights the waveform function keys, connectors, built-in quick help, operation keys, numeric keypad, knob, cursor arrows, and the channel setup button.
For more detailed product information on Trueform Arbitrary Waveform Generators, please visit:
何をお探しですか?