Comprehensive Testing of Fixed Wireless Access Devices

小冊子

Addressing the remaining residential need for broadband access using cabled infrastructure installation has become expensive and inefficient. FWA has emerged as a compelling alternative and robust solution to deliver broadband internet to these areas. With the latest advancements in Wi-Fi 7 and 5G, FWA can deliver similar levels of user experience as wired connections, and in cases with unimproved infrastructure, FWA could exceed overall network performance.

 

Keysight offers a comprehensive ability to test FWA devices. That entails benchmark performance testing under ideal conditions, real-world scenario modeling of the diverse and unpredictable nature of network usage, and special system tests like power outages, and Wi-Fi overload conditions.