M9472A PXIe 200W RF Interface Module

技術概要

The Keysight M9472A is a 2-slot PXIe, RF interface module for the M8920B Radio Test Set. The M8920B is well-suited for RF signals used by Land Mobile Radios (LMR) and Military Communication (MilCom) systems plus commercial connectivity standards (WLAN, LTE, 5GNR, Bluetooth®) that use wider bandwidths. The M9472A adds 200-watt input capability to the M8920B’s standard 50-watt input. The M9472A may also be used in conjunction with other PXIe RF test solutions that require high power input.