How to Make D-band Noise Figure Measurement with Signal Analyzer

アプリケーションノート

In the early 6G research, new sub-THz frequency bands have been explored especially the D-band (110- 170 GHz) for early research prototyping and system performance validation. For those early prototype systems, Noise Figure as one fundamental RF parameter would always be required to measure and characterize the performance of the whole system. Noise Figure is essential to verify new designs and demonstrate the device under test (DUT) meets specifications.