VSA 89600 Direct Data Connectivity Console Example

アプリケーションノート

Introduction

The DirectDataConnectivityConsoleDemo is an example program that shows the user how to configure the VSA’s .NET API to use direct data input to VSA. Like the WPF application, it sends data to VSA based on setting up the UserInput classes. The sending of data is simplified in this example since it is only sent on receiving a key input in the console window. Working through the entire console demo is achieved by the user responding to prompts in the console window. This demo guide will explain every step in more details.